Other Parts Discussed in Thread: TLV3601, BUF634A
Hello TI experts,
I would like to design a circuit to generate nanosecond pulses.
Is it any idea to let me start and studying in TINA simulation?
Here is my requirement:
- All system is based on 50 ohm.
- The pulse width must be adjusted between 1ns to 100ns.
- The rise time of pulse must be adjusted between 500ps to 10ns. (Maybe I can use a lowpass filter to limit the max 3dB frequency)
- The amplitude of pulse must be adjusted between 100mV to 5V. (Maybe I can use an external step attenuator to do it)
- The repetition rate of pulses is 100kHz.
Is there any block diagram or TI components to make this circuit?
I am looking forward to have some good suggestion.
Thanks.
SK.