Hello TI,
I am following some of greatest lab you have online. Now I am interested in OPAMP stability and I am watching "Precision Labs - Op amps: Stability".
We know that for stability of a system, the denominator of the transfer function must be ≠ from 0 (math is useful :D), which leads to loop gain different from -1 (AOL*ß≠-1 in case of an amplifier). I understand that the Phase margin tells how much the AOL*ß is close to -1.
Until here I am good, but when I have seen video 10.2 TI Precision Labs - Op Amps: Stability - Phase margin (8:07 picture bellow) I can not see why the phase margin is 5°. From the Gain graph |AOL*ß|=0dB and Phase(AOL*ß)≈0°. Putting this back to complex annotation gives AOL*ß≈1 and not -1. What I see is this example is 175° far from the instability point. Am I misunderstanding something?