Part Number: XTR117
Other Parts Discussed in Thread: XTR111, XTR115, XTR116
Hi,
is it possible to use the XTR117 in a 2/3 wire loop situation. The goal is to set for example an jumper to switch between 2 and 3 Wire.
In the 2 wire situation the XTR117 is connected as described in the datasheet.
In the 3 wire situation the Iret (Pin3) is disconnected and rest of the circuit is then connected to the 3 wire GND.
Is this possible? What are the implications?
If it is not possible is there a solution for that kind of situation? Is this maybe possible with the XTR111?
Thanks!
Best regards
Steffen