Other Parts Discussed in Thread: ADS124S08,
Hello,
I've got a bit of a confusing issue.
The circuit is a typical photovoltaic TIA, with Rf=2.4M, Cf=100pF, RLoad=100K. Output of opamp goes directly into an ADS124S08 ADC chip. System is biased to +/-2.5V. There are two additional ranges that can be switched in to the circuit using reed relays with Rf=24K and 240 Ohms, Cf to match the time constants across them all.
I'm reading ~200pA of dark current from the system. Voffset of the OPA392 seems to be around 4uV in this system, so I'd expect around 1.5pA as the minimum current readout at the 2.4M sense range. When disconnecting the photodiode from the board, indeed 0.5~1.5pA is the measured value, so leakage on the PCB is ruled out as a source. The photodiode is soldered directly to the PCB without a cable.
The system is at room temperature, around 20C. Photodiode is in a black cloth bag inside of a sealed metal container, no light in there at all.
We have measured a similar, but not exactly the same photodiode to have ~600fA of dark current using a keithley source-meter.
I'm somewhat new to very low signal level systems, could you help point out some reasons why the dark measurement is so much larger than expected? Schematic attached, datasheets linked.
Thanks,
zis
https://www.ti.com/lit/ds/symlink/opa392.pdf
https://www.ti.com/lit/ds/symlink/ads124s08.pdf
https://www.osioptoelectronics.com/Libraries/Datasheets/Photovoltaic-Photodiodes.sflb.ashx