Other Parts Discussed in Thread: INA240
I'm working with a customer to calculate expected accuracy in the system per below schematic.
Based on this being mid-supply architecture and them planning to use 100V/V gain device with Imax = 8.1A. I've calculated the below. Can you please verify if this is correct?
Vdiff = 2.5V / 100 = 25mV (assumed Vout is Vs/2) - should i take into account input value not being 0V? (I saw 3V full scale being reference in table 8.1 in datasheet)
Rsense = 25mV / 8.1A = 3mOhm
Prsense = 197mW
Vsense = 8.1A * 3mOhm = 24.3mV
Error_VOS = 5uV / 24.3mV = 0.02%
Error_lin = 0.01%
Error_gain = 0.33%
Considering those, it seems that total error is dominated by gain error, so per total error equation in datasheet, the error is effectively gain error due to external resistors or 0.33%.