This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA180: Large gain error

Part Number: INA180

Hi Team,

Our customer is having a problem with the INA180A1. According to the datasheet, the input resistances (Rint in Figure 46 in the datasheet) are equal 20 kohms, and connecting a RC filter (with R<10 ohms) on the input would not be a problem. In the customer application, they have used resistors 1 ohm in the input filter and got quite a large gain error. They measured the resistance between the noninverting input and ground, and the total resistance was arround 20.5 kohm, therefore Rint on the noninverting input cannot be equal to 20 kohm (more likely it's 0.976 kohm). Probably this is the cause of large gain error. Was this OpAmp changed in any way to get rid of the problem?

Can you please help?

Regards,

Marvin