Team,
Can you please help with the below questions.
Also can you please confirm for the RX only use case if it is acceptable not to apply power to PA_VS1/PA_VS2?
Since we will only need the RX path in the first step, some questions have arisen:
-If the 7-24V (PA_VS1) are omitted for the TX path, do various TX inputs, such as TX_PGA_IN, TX_F_IN(1/2), need to be pulled down to ground?
-Is it possible to pull these inputs directly to GND, or is a pulldown resistor needed?
-Are there any recommendations how to handle the resistor at PA_ISET?
Thanks in advance,
A.