Other Parts Discussed in Thread: LM7705, OPA365
Hi All
I am using LPC4357 series in my project. For the ADC part, I am using LMH6642. In this , ADC is showing some offset errors frequently. This offset varies with different boards. Some boards are working fine too. The 0-3.3V analog signal is given to LMH6642MF and the output is directly connected to MC. While checking voltage at the output of LMH6642, its showing correct value. But the digital value read by MC has some offset. In some board its working fine too. MC is changed a couple of times and the LMH6642 also changed and tried. In some board its working , so I am not doubting on software or MC.
Recently I made a new board and tested. It was giving exact values for ADC without any offset. But after two days, the same board started giving offset error. Still the voltage showing at the output of LMH6642 is correct. Without any ADC input, LMH6642 was giving around 20mV at the output. But ADC read by micro controller has an offset of 0.3V. After removing the power supply to LMH6642, the 0.3V offset was gone and the ADC gave 0V.
What could be the problem