Part Number: LM358
Hi,
What is the Vf of the ESD protection diode of the LM358?
Customers use in-circuit testers for PCB mounting inspection.
The VF of the input ESD protection diode of the LM358 cannot be read from the DS, but the test result was always about 0.8V.
However, in all recent tests, Vf = 1.2V.
I think the VF of a silicon diode is usually 0.7 to 0.8V, but is 1.2V the correct value for the LM358?
Looking at the latest PCN, the design / wafer size etc. have changed, but the DS specifications have not changed.
I understand that Vf = 0.8V can be 1.2V, but customers are worried that there may be major changes to the IC.
Best regards,
Hiroshi