Other Parts Discussed in Thread: TLV3501
Hello all,
Basically, I had lots of issues with the output ringing due to the fast response of the TLV3501, but I fixed that by increasing hysteresis and the use of the 1K-ohm output resistor.
The problem now is somewhat strange to me, and I think there is some sort of isolation issue between input and output. When the reference is set around midway around the pulse amplitude, the input signal is (...insert unknown word description ..), I guess replicated, delayed, or jitter-in the time domain ?
I've included a picture of what I'm talking about, look how the green-signal initially has a single peak before applying the reference (left picture) and then gets another peak when the reference voltage is applied/adjusted (right picture). The other two peaks are also effected similarly, but not shown in the snapped picture. When you run the oscilloscope continuously, you notice that the green signal is jittery, as well as the output. I need a clean output result for my application.
Possible concerns/questions I have:
1) The problem was slightly improved using Cbp1 and Rload.
2) How can I isolate the rising/falling edge of the comparator from the input ?
3) Rout improves the situation, but increasing it further will increase the output "falling-time"
Any suggestions ?
Thanks