This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6505: Power sequencing

Part Number: LMH6505

Hello,

I am powering an LMH6505 with two LDOs, one which regulates 6V to 5V, and one which regulates -6.5V to -5V. The part is upstream of a differential amplifier that is powered by the same rails. Currently, our power rails are coming up 75ms apart (6V and then -6.5V) which causes only the 5V LDO to regulate correctly while the -5V LDO output is 0V. When the rails are powered by a dual-channel power supply with minimal output delay, the regulators come online just fine.

Does this part have a specification for how much time can elapse between the different rails being powered?

Thanks,

Nicole