This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV7011: alternative solution to TLV7011DCKR

Part Number: TLV7011
Other Parts Discussed in Thread: LMV7239, , TLV3201

Dear e2e team,

My customer is using the TLV7011DCKR but there is no stock.

He would like to evaluate another solution (with stock, ~1k / 2k pcs) with the following features:

  1. Vcc (operative)= 3,3V (better if 1,8 ÷ 5V)
  2. Single channel
  3. Output type: push-pull
  4. Propagation delay: TpHL , TpLH <=  260 ; 310Ns (overdrive 100mV)
  5. Vio(offset) <= 8mV
  6. Vo :    Swing High max= Vcc- 0,3V  ;  Swing Low max< 0,3V
  7. Package  sot23-5  o   SC-70 (better)

Could you suggest any solutions?

Thanks,

Giorgia

  • Hello Giorgia,

    The closest drop-in replacement would be the LMV7239. It has the same pin-out, and is available in SOT-23 and SC-70.

    It is faster, so has x10 more supply current, and does not have the POR and the other enhancements of the newer TLV7011.

    The website shows plenty of the SOT-23, and the SC-70 expected this week.

  • Hi Paul,

    LMV7239 is too expensive for the customer compared to TLV7011.

    Do you have any other idea in mind?

    Thanks,

    Giorgia

  • Hello Giorgia,

    Sorry, the screen moved and I accidentally hit "Resolved". You may get a spurious notification.

    Is this a new design? Or a P2P replacement?

    Only the TLV7011 would satisfy the above requirements at 1.8V. And since it is a newer device on a cost efficient process, it is lower cost than the older devices. Other options are higher speed devices with higher cost.

    At 5V (2.7V min), you could try the TLV3201.

  • Giorgia

    We have not received a response on this post in a while, so we will be closing the post.  If you need further support, please reply or open a new post.  Thanks for your use of the E2E forum.

    Chuck