Part Number: INA233
Hi Team,
Can I assume that when I measure the input bias current on the positive input of a device, the input bias current on the negative side will be equal?
Thank you!
BR,
Stefan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: INA233
Hi Team,
Can I assume that when I measure the input bias current on the positive input of a device, the input bias current on the negative side will be equal?
Thank you!
BR,
Stefan
Hello,
Yes that would be a good assumption.
Regards,
Castrense
Hi Stefan,
the difference of input bias currents between the two inputs would be the so called "input offset current" and - to be honest - this input offset current isn't specified in the datasheet of INA233. So it cannot be guaranteed that the two input currents are equal. Similar, but not necessarily identical.
Also notice, that no maximum values for the input bias currents are given in the datasheet. Only typicals.
Kai
Hello,
Kai is correct there is no datasheet specification as well as them being similar, but not necessarily identical.
Regards,
Castrense