Hello everyone...
I am designing a current measurement circuit using a CT(current transformer, 5A/5mA, TA12-100).
The measured signal must be mapped into a 0-5V voltage signal for the microController's A/D to read.
However we must put a small resistance at the CT terminals, so what is the best conditioning circuit, that can translate these small voltages into amplified 0-5V.(using the LF411 or any similar device).
Can any one help me in this design.
Also any comments, advises well be highly appreciated...