hello,
I want to make short circuit protector with shunt monitor INA212. I make square wave current ,where impulse voltage is 12volts, impulse width 2ms. period from 7ms to 30ms. voltage that drops to shunt is 5mV, (I made experiment when shunt voltage was from 1mV to 60mV). In the shunt monitor out pin I have saw form signal. I want to get low or high signal from shunt monitor out pin, then I could continue my project.
where I can get more circuit example wtih shunt monitors?