Other Parts Discussed in Thread: THS4303, OPA656, OPA657
I try to use THS4303 as an active antenna amplifier, equivalent circuit of the antenna is a voltage source series with an 8pF capacitor. Input stage of the system is behave like an high pass filter I want to make the low cutoff frequency as low as possible. I am using single supply 5V and giving Vcm = 2.5V, What is the top limit value for Rt input resistance which is able to use?
When I didn't connect the 2.5V point in the single supply circuit which is being shown in the datasheet and measure the In+ an In- pins voltage, I saw 4V DC why I got this value?
I am waiting your answer as soon as possible
Thanks,