Other Parts Discussed in Thread: TINA-TI
Hello,
I have designed a peak detector circuit with OPA 659. My purpose was to measure the peak of the fast (about 300 kHz) signal. Therefore I connected the output of the opamp to microcontroller ADC. In order to get more accurate results, I averaged 20-50 values of ADC samples.
However the results for fast signal were not true. For example, when I intended to measure 1000 V I got 1400 V from the microcontroller. I guess my opamp output reaches even higher than 1400 V because of averaging. (It worked fine with dc values.)
I think the reason for that is my opamp rings or overshoot the values.
What could be the reasons for this situation?
What should I do to solve it?
I attached my schematic below.
Sincerely,
Behtan Umut Mercan