This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRF1208EVM: Quick Question

Part Number: TRF1208EVM
Other Parts Discussed in Thread: TRF1208, AFE7950

Hi team, I wanted to confirm that there wasn't an EVM populated / setup for demonstrating the transmit chain shown in section 8.2.2? I think the only EVM we have is setup for the receive chain (8.2.1)?

Thanks,

Cam

  • The TRF1208 is tuned for the RX chain, Single-ended to Differential. However, the TRF1208 is constructed as an fully differential amplifier that can be set-up for both the RX and TX chain. We do have data showing AFE7950 + TRF1208 in the transmit path, but the data hasn’t been public posted performance data yet. I'll send you an email separately