Part Number: OPA4990
1. Is the short-circuit current of +/- 80mA for 4 channels or each channel?
2. When the load increase, this current will decrease, right?
3. How will the open-loop output impedance affect on the max load current?
4. Does the X2QFN have exposed pad for thermal? Is there a layout example for this package?
5. Does TA(specified temperature) in section 6.3 refer to ambient temperature?
Thanks