Dear Team,
Please help to reply to the following question. The waveform raw file as enclosed.

Many Thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Jimmy,
Can you provide the full schematic, showing the input signals and the MOSFET?
Also, what is the exact part number of the MOSFET? Gate capacitance? Threshold?
Is the top zoom channel the output? It looks like it is coming down from 4V, which is above the 3V supply.
Jimmy
We have not received any new information on this post and will be closing it. If you need further support, feel free to reply or open a new post.
Chuck