Part Number: TLV3202
Other Parts Discussed in Thread: TLV3201
Hi,
I am doing the simulation with TLV3201.
IN+: Pulse signal with 2MHz
IN-: Vref at 2.5V
Following hysteresis setting on datasheet Figure 29.

The output result is giving unexpected output and doesn't follow the hysteresis setting 1.675V trigger low, 3.325V trigger high.

Kindly comment what is the issue happen?
Regards,
JJ