Part Number: PGA281
Hello,
We are planning to use PGA281 for high accuracy voltage measurement. The minimum input voltage is 350 mV and the signal will be unipolar. The gain of PGA281 will be selected as 4. The datasheet shows the offset voltage, offset voltage error, and Gain error for +/-15 V input supply.
Is it possible to use PGA281 with only 5V supply? if yes, can we use same offset voltage, offset voltage error, and Gain error for tolerance analysis as mentioned in datasheet for +/-15V?
Is it possible to use PGA281 with only +/-5V supply? if yes, can we use same offset voltage, offset voltage error, and Gain error for tolerance analysis as mentioned in datasheet for +/-15V?
Regards,
Ram