Other Parts Discussed in Thread: TINA-TI, IVC102
Hello,
I'm trying to evaluate ACF2101 against the conventional T transimpedance amplifier in terms of noise reduction.
As a first step I'm trying to simulate the ACF2101 in LTspice, however I'm issues with getting the output right.
- The output more or less stays at 8.44V (instead of starting at 0V)
- The integration of the output doesn't happen when Hold pin is ON
- Though the input current is positive the output voltage isn't negative
I have considered the timings for fs=10kHz



I have gone through the other posts but didn't seem to help.
Any support in identify the mistake or change required to get the simulation working would be helpful.
Thank