Hi, I am designing a 1MHz buck converter, can you please recommend an amplifier that is fast enough? high side is better, but low side is also acceptable.
Thanks,
Shengnan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Shenganan,
You can use this filter in our product search.https://www.ti.com/amplifier-circuit/current-sense/analog-output/products.html#p314=800;1300&sort=p314;desc
Like you saw in our product search you have to dig into the details. I would recommend the INA296A, INA296B, INA241A, INA241B. The INA290, INA280, INA293 and INA281 have the same issue you saw in your other post as they have the same architecture.
Hi Shengnan,
keep in mind, though, that when installing an OPAmp within the feedback loop of a converter the phase margins of OPAmp and converter can be eroded eventually resulting in instability. In this case you should perform a phase stability analysis of the circuit.
Kai
Hi, Javier, with INA241, it says support switching frequency up to 125kHz, what does that mean?

Hello Shengnan,
This is the VCM switching frequency for a PWM system. This is due to the Enhanced PWM rejection limitations.
Hi Shengnan,
keep in mind that the datasheet of INA241 is incomplete so far. As being a new device the datasheet only contains advance information. Many specs and figures are still missing.
Kai