Part Number: TLV9161
Hi Team,
We want use OPA or comparator as offset function. Can our OPA achieve below requirement? We want output = intput+1V. For example, Vin = -1V~3.3V Vout = 0V~4.3V

Regards,
Roy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kai,
We don't have schematic because we have no idea which chip can achieve our requirements.
Roy
Roy,
30MHz is fairly fast. The edges are much faster, do you care about edge widths?
What is the bandwidth needed? What are the input and output load impedances?
Are you sure +1V is the only or best solution? A more detailed problem explanation might lead to a different type of solution.
Hi Ron,
Our signal frequency is around kHz level.
Before, we try to use OPA to achieve the requirement, but OPA BU also suggest use comparator. Do you have any suggestion?

Regards,
Roy
Hi Roy,
this would be the job for a fast comparator:
https://www.ti.com/amplifier-circuit/comparators/products.html#sort=p83;asc
Kai
Roy,
I would suggest 2:1 analog switches. Available in 4 or 6 channels.
https://www.ti.com/switches-multiplexers/analog/products.html#p1143=2:1%20SPDT&p480=4;6