Other Parts Discussed in Thread: OPA353, OPA350
Hi guys,
As mentioned in my last threads, I'm working on designing a circuit for TI to measure the current consumption of MSP430.
My Idea is to connect a shunt in the supply line of the target MSP430 and measure the voltage drop across it. Now I have to take care about the voltage regulation. I think about using an op amp (voltage follower) and connect the shunt inside its feedback loop. The problem is that most op amps are not stable while driving cap load (10uF and 100nF at the input of MSP430). I read several TI articles about compensation of op amps to get stable while driving cap loads.
My question now is: Is there any TI op amp which is already compensated? Do you suggest any compensation lead for any special op amps?
I attached my simulation to understand what I'm talking about:
http://www.fileswap.com/dl/WXQLltte/mspbeginner_op_amp.TSC.html
Regards