This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA296A: What is the input impedance?

Part Number: INA296A

I couldn't find this parameter in the datasheet. what is the input impedance of INA2xx series ?

Here is an example for and LT amplifier.

  • Hello Shengnan,

    We normally don't have this as a specification as it does change for each gain.  The number below are typical and not guaranteed and can vary from device to device.  The final datasheet should have a typical curve of IB vs Vsense.  

    INA296A1: 50kΩ

    INA296A2: 25kΩ

    INA296A3: 10kΩ

    INA296A4: 10kΩ

    INA296A5: 5kΩ