Other Parts Discussed in Thread: TLV6742,
Hello, I received the following question from a customer:
"I wanted TI to confirm and check the Differential Input impedance on the OPA2375 and TLV6742 datasheets. The input impedance for the Differential mode is 10MOhms and the Common mode is 10GOhm. 10MOhm for the differential input impedance seems low for the op-amps. Can this be confirmed to be true based on the datasheet?
Additionally, with the max 1mV max offset voltage / 10Mohm differential input impedance would have 0.1nA of leakage current. Would this leakage current be correct?"
Thanks!