Hi,
The footprint of INA333HKQ on the web site Ultra libraria looks inverted compared to the 3D model and the datasheet:
Could you confirm that pin 1 is at the top right corner when the part is mounted?

Kind regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The footprint of INA333HKQ on the web site Ultra libraria looks inverted compared to the 3D model and the datasheet:
Could you confirm that pin 1 is at the top right corner when the part is mounted?

Kind regards
Hi Eric,
Could you confirm that pin 1 is at the top right corner when the part is mounted?
Yes, it seems that there is a mix-up somewhere. If it is INA333SHKQ package from the top view, the pin #1 should be shown on the right side, see the image below, which I captured from mouser.com.
INA333SJD package has different pin out, pin #1 should be located on the upper left corner from the top view.
INA333SHKJ package should have the identical pinout as in INA333SHKQ based on the drawings in the datasheet (from the top view).


I will ask our system engineer to revisit these drawings and revise it in Ultra Librarian.
Thanks for pointing out the mistakes!
Best,
Raymond