This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS4271 OPAMP 5V Single Supply and AC Coupled Configuration.

Other Parts Discussed in Thread: THS4271, THS4303

Hi,

I want to use THS4271 OPAMP with 5V Single Supply and AC Coupled.

The equivalent circuit of the source is signal source series with  8pF capacitor. I need 500kohm input resistance to reach my low frequency goal.

I am using THS4271 (SOIC) as buffer I selected Rf resistance value 200ohm, I am using split resistor technique for biasing  and I chose Split resistor values R1 and R2 1Mohm because of to get 500kohm input resistance.  Could you verify my circuit or suggest an alternative circuit to me?

Thanks,