Other Parts Discussed in Thread: OPA350
Dear all,
I have 0.005Ohm current sense resistor.
What's the best differential amplifier to measure the current (max 1A).
Specifications
1) High side current measurement
2) The bus voltage is 48V while the Op-amp would be supplied by 5V.
3) need to measurement the current in both the directions
OPA350 is suitable for this application?
V=IR Drop across current resistor = 0.005*1 = 5mV, this is very small voltage
Any referense schematics would be of great help.
Thanks and regards
Ramakrishna