Part Number: THS4631DGNEVM
Hi Team,
Using THS4631DGNEVM as a non-inverting amplifier with a gain of 2. I am sending a -5V to +5V signal which will be amplified to -10+10V. However, I would also like to add a DC bias so that the output signal is 0V to 20V. I cannot add the bias signal to the input waveform, so I am trying to see if there is a way to add a DC bias voltage to the amplifier or inputs (such as a summing amplifier configuration) that would achieve this.
Thank you.