Other Parts Discussed in Thread: AMC1300
Hey Team,
Could you help me out on getting some information on a TI part. For the AMC1301, the datasheet shows that it has short circuit protection on the output is up to +/- 13mA and an output resistance of <0.2Ω.

- Can you explain in a little bit more detail on how the output short-circuit protection works? I looked under the fail-safe section of 9.3.2 but it didn’t say much about the output current.
- How does the output resistance change whenever short-circuit protection is occurring?
- Can the output current transiently exceed +/-13mA? For instance, let’s say if it went to +/-30mA for 100us?
- For the inputs, can the differential voltage be 250mV with a common mode (Vcm) of -250mV (V+= -135mV and V-= -385mV)?