Other Parts Discussed in Thread: OPA564,
I want to find a driver for this DFB laiser, whose parameters are listed as below.

The triangular wave is used as the input to control the Laser, whose frequency is almost 100KHz.
You can have a look at the trianglular wave, listed as below.

According to the SPEC of OPA564, is it possible for this laser working with the current being 500mA and the voltage being 1.8V?