你好,芯片供电:V+连接+100V,V-连接-12V,是否合理?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Rengui,
芯片供电:V+连接+100V,V-连接-12V,是否合理?
Yes 合理. The recommended operating voltage is ±75Vdc for a symmetrical dual supply voltage rails, and the total Vs delta, Vs = V+ - V- = 150Vdc (the absolute max Vs. supply is <160Vdc).
With V+ = 100Vdc and V- = -12V, Vs = 100 - (-12) = 112 Vdc <= 150Vdc, which the asymmetrical voltage supply rails are safe to operate without issues.
Below is the input common mode voltage requirements, where input voltage has to be: -11V < Input_voltage < 97V per the asymmetrical supply rail requirements (for linear operation and behaviors).
If you have additional questions, please let us know.
Best,
Raymond