Part Number: INA237
Hi team,
I have connected eight (INA237)devices in a single bus. I doubt it will affect the racing time.
What are the Pin Capacitance (SDA, SCL) and the total capacitance of one bus line Cb?
Thanks, Regards
Anoop Varma m
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: INA237
Hi team,
I have connected eight (INA237)devices in a single bus. I doubt it will affect the racing time.
What are the Pin Capacitance (SDA, SCL) and the total capacitance of one bus line Cb?
Thanks, Regards
Anoop Varma m
Hello Anoop,
The total max capacitance of one bus line is an I2C protocol specification, and our device works with the standard I2C protocol. That being said, the max bus capacitance could depend on which MCU you are using and any other devices you have on the bus, as well as the speed you are communicating at.
I have tested 4 devices on the bus with 4.7KΩ pull up resistors, running in High Speed mode without an accelerator, and had zero issues. I don't think 8 would be a problem, but that really depends on your frequency/MCU etc.