Hi TI,
I use the INA240A3 to measure the inductor current in CCM BUCK topology which switch frequnce is 300KHz.The INA240A3 is placed on the high side.Then I found the output wave of the INA240A3 is very strange.
I know the BW of INA240 is 400KHz(-3dB).Theoretically the output should be a triangle wave even its amplitude is attenuate. However its output wave surprised me, yes it did surprised me.
This is the surprising wave.
Here is the condition:
vin = 30V
vout = 9V
load current = 5A
Here follows the schematic
So,could you tell me why the output is so strange?