The datasheet for the LM747 dual-opamp lists only typical values for Transient Response: Rise Time (0.3 µS) and Overshoot (5%). Is there a reason why no maximum values are given here? We have 2 lots of TI (then National Semiconductor) LM747H chips. One lot, manufactured in 1984, has observed rise times of 0.16 - 0.20 µS with overshoots of 3.5-6%. The other lot, manufactured in 1994, is showing similar rise times, but has observed overshoots of 18-20.5% for all units with similar rise times as the other lot.
Is there a reason why such a discrepancy in overshoots would exist between two of (what should be) the same lots of parts? And since the 5% listed in the datasheet is only a typical value, is a ~20% overshoot actually an issue with the part itself? Unfortunately, I don't know the end-use application, so I can only speak in terms of the chip itself, now how it will act in its final circuit.
Thank you,
Tyler