This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMV324: Operation under VCC~5.5V

Part Number: LMV324

Hi team,

In the datasheet of LMV324, it says that both “Absolute Maximum Supply Voltage” and “Recommended Operational Condition of Supply Voltage” are 5.5V.

But in many op amps, abs. max. supply voltage is higher than recommended maximum supply voltage.

So, my customer is wondering if it works with typical VCC=5.5V.

They understand that TI should not guarantee that.

They are considering to use the LMV324 with the power supply at 5.5V +/- 0.2V.

Do you think LMV324 works in this condition?

Regards,

Ohashi