Part Number: OPA192
Hi team,
My customer use OPA192 in their project. And they meet below issue, could you please help give some comments? Thank you!


Regards,
Ivy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPA192
Hi team,
My customer use OPA192 in their project. And they meet below issue, could you please help give some comments? Thank you!


Regards,
Ivy
Hello Ivy,
I suspect the jitter is actually noise being added to the fast slewing input voltage applied to the amplifier circuit. The circuit has a number of high resistance resistors that will directly generate significant thermal voltage noise, or generate voltage noise converted from the op amp's input current noise flowing through the resistances. Of particular interest are the two 500 kilohm series input resistors through which the OPA192 input op amps input currents flow. Each side of the circuit contributes noise in root-sum-square manner.
I suggest an experiment. Scale the 500 kilohm input resistors down to 50 kilohms, the 4 kilohm resistors down to 400 Ohms, and increase the 100 pF capacitors to 1 nF. Short out the 3.92 kilohm resistors as all they are doing is adding thermal voltage noise to the circuit. Then, test the circuit and see if the jitter decreases. The resistors in the OPA192 output stage could be scaled as well, but try the experiment on the input stages first.
Regards, Thomas
Precision Amplifiers Applications Engineering
Hi Thomas,
Thanks for your comments.
Because it is a project that's already in production, and we replace competitor device in this project.
So the customer don't like to make too much modification, such as the input and Rf resistor.
In addition, the customer think increase the capacity will affect the rise rate, they need a fast rate of rise.
Besides, from below figure, we can see the bandwidth in G=100 is about 100kHz.

regards,
Ivy
Hi Ivy,
please explain what DC potentials are connected to "A-" and "A+". Where exactly is the ramp applied? How is the ADC with its charge bucket filter connected to the last OPA192? Can you show a complete schematic of this section?
Kai
Hi Ivy,
Please provide a like image for points A and B with the competitor's op amp in place of the OPA192. And the information Kai has requested is needed for a more meaningful assessment.
Regards, Thomas
Precision Amplifiers Applications Engineering