Other Parts Discussed in Thread: TLV3604
LMH7324 - autosave 22-05-12 18_17.TSC
I am going to use lmh7324 to convert and output LVDS signal. The evaluation manual has written the following description:
This demo board can operate with a simple dual supply of ±2.5V. The output voltages are now about
1.35V and 1.0V and comply with LVDS and RSPECL levels
But I use Tina simulation but it doesn't work properly. Why. If the VCCI is increased to 3.3V, it can work normally
Thank!!!