Part Number: LM358
Hi Experts,
A customer is using LM358P as a comparator and they encounter an issue that is heating up the device and the lifetime average is roughly 48 hours.
The connections are described below:
Supply voltage: Ground/+12-13V DC
IN1-: connected to 700 Ohm
In2+: connected to 1kOhm potentiometer (Ground/+12V)
Out1: connected to a Power Mosfet Transistor
In2- and In2+: connected to Ground
Out2: no connection
Can you help? Thank you in advance
Regards,
Marvin