Part Number: THS4521
Other Parts Discussed in Thread: ADS4245, , THS4551
Hello,
In my project, I am using two ADC drivers THS4521IDR and an ADC ADS4245 and I would like to know how to connect them properly.
The input signal of the drivers comes from an Operational Amplifier and it is single ended.
- Should I connect the Operational Amplifier output to the positive input of the Driver?
- If I connect the Operational Amplifier output to the negative driver input, will I have the ADC output inversed or will I get a completely wrong signal?
How should I connect the positive and negative driver outputs to the ADC (ADS4245 )?
- Positive output to positive input and Negative output to negative input? I ask this because in the datasheet of another driver datasheet (ADA4940) the connection is positive to negative and negative to positive. Please, see next picture:

Could you tell me if my circuit is correct (please, note that the positive driver output is connected to the negative ADC input and the negative driver output to the positive ADC input)?

If you need further information, do not hesitate to consult me.
Thank you very much in advance.
Have a nice day,