This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS3092: THS3092 EVM Bill of Materials

Part Number: THS3092


Hi team,

According to Table 3 of the datasheet, it seems that 22uF cap is used for C1/C2. But the part number, TAJD685K035R is 6.8uF. 

Could you tell which is used in the EVM correctly?

Regards,

Noriyuki Takahashi

  • Hello Takahashi,

       Thank you for catching the error in Table 3. C1/C2 are decoupling capacitors for the power supplies to the device, and we would recommend these capacitors to be equal to or larger than 6.8uF. Both values will work, but I would suggest to use the part number TAJD685K035R which is 6.8uF. 

    Thank you,

    Sima