Part Number: TLV9152
Other Parts Discussed in Thread: , UCD9090
Hello,
We read in the datasheet that a pull-down was present on the shutdown pin.
We intend to do the following schematic to ensure we have no voltage on our CPU until the 3V3 is present (3V3_aux is present way ahead).

The output of the UCD not being piloted until the POR is ended, we want to put an external pull-up to P3V3_aux on the signal that drives the shutdown pin.
However, the datasheet does not provide information on the pull-down value, only a typical current over the whole voltage range so it's not helping much.
Do you have more information about it ?
Is a 10k on R1 enough to ensure the TLV9152 is shutdown at board startup until the UCD drives a 0 logic level ?
Best regards,
Clément