This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Our customer is looking for a pin-for-pin DIP alternative/upgrade for LM318-N to be used for a British Fidelity MVT. The product page only suggests LM318 as an alternative, however, they are identical and offers no upgrade.
Can you help suggest a part?
Thanks in advance.
Regards,
Marvin
In the DIP package, there are no fully compatible alternatives. The nearest would be the TLE2071(A), which has a lower slew rate.
Hey Marvin,
There is a new device released recently, the OPAx992, which was made with audio performance in mind. This is a 40V device with lower BW and Slew rate but outperforms the LM318-N in most other categories. I've provided a comparison table below.
► Part Number | lm318-n | opa992 |
Manufacturer | TI | TI |
Channel Count | 1 | 1 |
Vs Range | 10V to 40V | 2.7V to 40V |
GBW (MHz) | 15 | 10.6 |
Slew Rate (V/µs) | 70 | 32 |
Vos max @ 25oC (mV) | 10 | 1 |
Vos Drift, typ (µV/oC) | 6 | 0.25 |
Rail-to-Rail | No | In, Out |
IQ typ (mA) | 4.5 | 2.48 |
VN (nV/√Hz) | 15 | 7 |
ISC typ (mA) | 20 | 65 |
IBias (typ) (pA) | 150000 | 10 |
Operating Temperature (°C) | 0 to 70 | -40 to 125 |
Best,
Jerry
Hi Jerry and Clemens,
Thank you for the recommendation. the customer has a follow up regarding this.
They already have an OPA2227P and OPA228P on hand, would it be okay to use these as a substitute for the LN318N and TL074?
Thanks!
Regards
The OPA2227 is a dual opamp. The TL074 is a quad opamp.
The OPA228 is somwhat slower than the LM318, and decompensated. I do not know what electrical characteristics you actually need.
Marvin,
If you could provide system specs needed we can help you find a good replacement or verify if OPA2227/OPA228 would suit the customer needs.
Best.
Jerry
Hi Marvin,
the datasheet of LM318-N shows in figure 37, 38 and 41 three different compensation methods. This makes the LM318-N rather unique. If the circuit of customer is using one of these compensation methods, it will be very difficult to find a fully exchange-compatible OPAmp. But if the customer is not using these compensation methods or is willed to make layout changes, then there are a lot of compatible OPAmps.
I would eventually take the NE5534. As the LM318-N is usually taken in high gain applications, the NE5534 would not need to be compensated then.
A more concrete answer can only be given when seeing the schematic.
Kai
Hi All,
Thanks for the support. The customer is looking to replace the LN318N and TL074 on his British Fidelity MVT audio Preamp. I was unable to find schematic or the spec of this device due to it's old age.
Regards,
Marvin
Marvin,
Understood, so they are looking for a 1:1 drop in replacement. We do not have a newer drop in replacement for the LM318-N.
Best,
Jerry