This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMV225: θJt

Guru 11525 points

Part Number: LMV225

Hi team,

Could you share the θJT data for LMV225SD/NOP ?

Sincerely.
Kengo.

  • Hi Kengo,

    Please find the Thermal Metrics below for LMV225SD: 

    Thermal Metrics (1)
    Theta JA-High K (2) = 90.9 °C/W
    Theta JC, top (3) = 81.3 °C/W
    Theta JB (4) = 60.6 °C/W
    Psi JT (5) = 4.0 °C/W
    Psi JB (6) = 60.8 °C/W
    Theta JC, bottom (7) = 11.2 °C/W

    (1) For more information about traditional and new thermal metrics, see the Semiconductor and IC Package Thermal Metrics application report (SPRA953).
    (2) The junction-to-ambient thermal resistance under natural convection is obtained in a simulation on a JEDEC-standard, High-K board, as specified in JESD51-7, in an environment described in JESD51-2a.
    (3) The junction-to-case(top) thermal resistance is obtained by simulating a cold plate test on the package top. No specific JEDEC-standard test exists, but a close description can be found in the ANSI SEMI standard G30-88.
    (4) The junction-to-board thermal resistance is obtained by simulating in an environment with a ring cold plate fixture to control the PCB temperature, as described in JESD51-8.
    (5) The junction-to-top characterization parameter, ΨJT, estimates the junction temperature of a device in a real system and is extracted
    from the simulation data for obtaining RθJA, using a procedure described in JESD51-2a (sections 6 and 7).
    (6) The junction-to-board characterization parameter, ΨJB estimates the junction temperature of a device in a real system and is extracted
    from the simulation data for obtaining RθJA , using a procedure described in JESD51-2a (sections 6 and 7).
    (7) The junction-to-case(bottom) thermal resistance is obtained by simulating a cold plate test on the exposed (power) pad. No specific
    JEDEC standard test exists, but a close description can be found in the ANSI SEMI standard G30-88.

    Regards,

    David Chaparro