Part Number: INA1620
Dear mr.
I would like have bridge output with INA1620. Please se picture below,
Is it right and can I use two half of one IC ?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: INA1620
Dear mr.
I would like have bridge output with INA1620. Please se picture below,
Is it right and can I use two half of one IC ?

Thank you for fast answer.
Please look to another variant,
Witch one is better? (short-circuit protection I 've remember)

Hi Mikhail,
it's not simply better or worse. It's just different. The first uses a differential input signal and the second not. There are many other ways to generate a differential output signal, by the way.
Kai
Hi Mikhail,
Kai is correct. Both implementations are fine. We have an application note that discusses the second proposal. Either implementation will work.
Best Regards,
Chris Featherstone