Other Parts Discussed in Thread: LMH730033
A question about using the LMH6503 VGA in a high impedance application.
In the app note AN-1808 LMH730033 Eval board, this is a circuit listed page two. It is meant as a 50ohm load to the preceding stage.
If one wants to use this circuit at at higher load impedance (with the same noninverting single ended input configuration) and R1 becomes 1kohm, does R2 need to follow suit? Or is it ok for R2 to stay at 50ohms?