Part Number: BUF602
Other Parts Discussed in Thread: TPS65133, FDC2214, TINA-TI
Dear TI experts,
I have two questions about powering the BUF602.
First question, can I power BUF602 with TPS65133?
The TPS65133 is a ±5V output dual-rail DC converter with a maximum output current of 250mA for the positive and negative channels, respectively.
The second question is about the power consumption of the BUF602.
Since my system is battery powered, how is the power consumption of the BUF602 calculated?
The signal that needs to be buffered is a half-sine wave with an amplitude of 1.8V output by the LC tank of FDC2214.
Best regards,
Will